Other Parts Discussed in Thread: TL052A, LM358B, LM358BA
Hi Engineer,
When the test found that the input was unchanged,
a new batch of TL082CDR was used, and the output PIN output was low (normal Io voltage to ground is 0.55V, low Io = 0.51V), and replaced with TL082CDR one year ago , Out PIN increased to normal, the entire product test can pass.
As long as it is this batch of materials, there will be problems as soon as it is powered on;
The following is the circuit schematic, please help review.
Thank you
Best Regards
Elsa Duan