Hello,
+VCC1, +VCC2, -VCC1 and –VCC2 can be powered up in any order?
Best regards,
K.Hirano
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
+VCC1, +VCC2, -VCC1 and –VCC2 can be powered up in any order?
Best regards,
K.Hirano
Hi Kazuhiko,
please read section 11 of datasheet:
"Operate the two positive supply pins and the two negative supply pins at the same
voltage. Using separate sources on the two pins risks forward-biasing the on-chip parallel diodes connecting the
two supply inputs together. +VCC1 (pin 13) and +VCC2 (pin 16) have two parallel diodes that are normally off if
the voltage at the two pins are equal. The same is true for –VCC1 (pin 8) and –VCC2 (pin 5)."
And:
"The recommended external supply configuration brings ±VCC into the output stage first, then back to the input
stage connections through a π-filter comprised of ferrite beads and added decoupling capacitors at +VCC2 (pin
16) and –VCC2 (pin 5). Figure 106 shows an example decoupling configuration."
Kai
Incidentally, the separate supply connections for the output stage and input stage simulated to show incrementally improved HD performance vs using only one supply pin - that showed up in the full package model simulations.
Those Ferrite beads are not really 4uH inductors as shown, but lossy inductive elements, you might look at the EVM BOM to get a part number.