This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2835: Naming

Part Number: OPA2835

Hello, 

1. In the OPN, OPA2835IDGS, DGS stands for the package, right?

2. Does "I" have any meaning? It seems that all part numbers listed in the datasheet all have "I"

Thank you!

  • Hi Elisha,

    to 1: See the "packaging information" in the "package option addendum" of datasheet.

    to 2: " I " stands for the "extended industrial temperature range" of -40°C...+125°C. The standard "industrial temperature range", on the other hand, usually ranges from -40°C to +85°C.

    Kai