Other Parts Discussed in Thread: INA215, INA293
Hi expert,
Do we have a INA138 pin to pin device that has higher accuracy?
Total current error requirement: <50mA
Power supply: 5V Vcc
Common mode voltage: > 20V
Sense current: 5A(max)
Sense resistor: 5 mOhm or 10 mOhm
I see the accuracy of INA215 is much better. Is this a good choice if the customer can accept a not pin to pin device?