Hi Expert:
My customer is using the INA181A2 for the low side current measurement in the inverter, please see the schematic attached.
The issue is the inherent gain of INA181 is 50v/v , and customer put the external 1k resistor on the input of INA181, and the estimated gain is 45V/V,
However the actual gain is 22V/V (Vin = 103mV , Vout =2.2V) in the normal working , and the actual gain is 7V/V (Vin = 675mV, Vout = 4.7V) in the short current mode.
Could you please explain the reason ?
Thanks!