Other Parts Discussed in Thread: INA326
Hi Team,
Here is an inquiry from a customer.
Please tell me if there is a version of the INA826 with an input range higher than 1V below supply. The INA826 maximum input is 2.3V when powered on 3,3V, I need to accommodate a 2.50V input. The input range of the INA826 is limited to 1V below its positive supply, 3.3-1 is the 2.3V.
Do you any suggested device that fits this specfications?
Regards,
Danilo