This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RC4559: Replacement for 4739 dual op amp (audio)

Part Number: RC4559
Other Parts Discussed in Thread: RC4580, TL081, TL071

Hello,

I'm searching a replacement for the 4739 dual op amp (vintage guitar effect).

I think the RC4559 should be a good candidate, it's pretty similar. The pin-out is different but it's not a problem.

Is there any other component similar enough to replace the 4739?.

I attached the datasheet.

Thank you.

  • Former Member
    0 Former Member

    Hi Thierry,

    Which 4739 are you referring to?  Does it have a prefix?  If you can find out, then I might be able to make a better suggestion.

    If you're looking at the RC4559, then you might also consider the RC4580.  It's a popular audio amp at a lower cost.

    Regards,

    Daniel

  • Hi Daniel,

    Thank you for your reply.

    The RC4739; that's it.

    I'm looking for the closest possible replacement in terms of electrical values.

    I mean: same Input Offset Voltage, same Input Offset Current, same Bias Current, same Slew Rate, etc...

    The pin-out does not matter.

    I'm not interested by RC4739. I want a current production op amp.

    Regards,

    Thierry 

  • Hi Thierry,

    if little supply current is important, I would go for the RC4559.

    Kai

  • Hi Kai,

    Thank you for your reply.

    I'm looking for a model that comes closest in terms of sound.

    I know it would be easy to buy an NOS R4739.

    I want to use it in a jazz guitar preamp and keeping the R4739's mojo is really important.

    Regards,

    Thierry 

  • Hi Thierry,

    can you show a schematic?

    Kai

  • Former Member
    0 Former Member in reply to Thierry Baj1

    Hi Thierry,

    Unfortunately, nothing will have the exact same specs as the original amp.  I would think the THD and noise performance of the amp would be the most important factors in determining audio quality.

    However, unless you just want the cleanest THD+N/noise performance, it's going to be virtually impossible to decide which has most nearly got the R4739's "mojo."

    Here's what I would do, pick a few different parts and order some samples.  Plug them into your board and see which you think sounds best.  I would try RC4559, RC4580, and potentially the TL071 and TL081 devices after that if needed.

    Regards,

    Daniel

  • Hi Daniel,

    I fully agree with your recommendation to alternatively use the TL071, because the TL071 has much lower input noise current compared to the bipolar OPAmps. This can be advantageous when being directly connected to the pick-ups. That's why I asked for the schematic :-)

    Kai 

  • Former Member
    0 Former Member in reply to kai klaas69

    Good suggestion Kai.  Let's see what Thierry will share.

    Daniel

  • Hi Daniel and Kai,

    Thank you for your help.

    I also think the THD and noise performance are the most important factors.

    From the RC4739 datasheet:

    <0.05% distortion into 2kOhm load

    10nV/√Hz noise at 100Hz

    I don't see theses parameters in the RC4559 datasheet.

    Thierry

  • Hi Thierry,

    the noise can be calculated from this data:

    Divide the numbers by SQRT (20kHz - 20Hz) = 141 x SQRT (Hz). This yields 9.9nV / SQRT(Hz) and 0.18pA / SQRT(Hz).

    Kai

  • Former Member
    0 Former Member in reply to Thierry Baj1

    Hello Thierry,

    As for THD performance, I'm afraid you're right in that the RC4559 does not have anything in the datasheet.  Keep in mind, this part is almost 40 years old now.

    The older noise parameters were often given as integrated values rather than as a broadband spectral density.  For the sake of this example, Kai's calculation is good for comparison's sake.  You can learn more about this topic in the TI Precision Labs Series on Op Amp noise.  Here's a link to video 2 and video 3, which I think you'll find most helpful.  You can use the information in this slide to calculate the integrated noise for the RC4559.

    Regards,

    Daniel

  • Thank you very much for Daniel.

  • Former Member
    0 Former Member in reply to Thierry Baj1

    Hi Thierry,

    I'm happy to help and hope you found this information useful.  I know it can be somewhat frustrating trying to work with older parts.  Please, let us know if you have any further questions.

    Regards,

    Daniel

  • Hi Thierry,

    I think the distortion of RC4559 should be very similar to the RC4739, maybe even a bit better.

    Kai