This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMV342: oscillation issue

Part Number: LMV342

Hi,

There is oscillation issue in LMV342.

Could you let me know why oscillation is occurred?

Below is the circuit.

AVDD is 3.3V

Vref_L is 0.825V

I'm not sure what R70 and R98 is for.

But when R70 is 240kOhm, U9A output is oscillated as below.

When R70 is 0, output is as below.