Hello all,
I have a requirement for my analog inputs to protect it against overvoltage up to 60V.
The continuous input current in THS4531 is 10mA so can I put a series resistor to limit the current in 60V overvoltages?
The required gain is 0.5V/V
So can I put these resistors
Rg=7.5k (0.5W)
Rf=3.75k
If I want to use a smaller resistor in input can I use :
Rg=15k (0.25W)
Rf=7.5k
Rf is some kind of big then do you think if it is acceptable?
Best regards,