Hi,
I'm using AMC1100 analog isolator for current sensing application.
input side of the amplifier is connected between 5V and ground_1 and output side is connected between 3.3V and ground_2.
there is a voltage difference between ground! and ground_2
ground_2 is 70V above ground_1
Will AMC1100 work is such a configuration? what are the points to consider?