This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV2313-Q1: Min/Max Values on Vos, Ib, etc.

Part Number: TLV2313-Q1
Other Parts Discussed in Thread: TLV2316-Q1, TLV9002-Q1, TL972-Q1, TLV9062-Q1, TLV272-Q1

Hello,

I'd like to ask for some information about TLV2313-Q1.

  • Min and Max values on VOS - Input offset voltage over full temperature range (TA= -40 to 125 °C)
    • If you refer to dVOS/dT, please share with me at least the Max value of the dVOS/dT.
  • Min and Max values on IB - Input bias current over full temperature range (TA = -40 to 125 °C)
  • Max value on VO - Voltage output swing from supply rails over full temperature range (TA = -40 to 125 °C)

If Max and/or Min values are not available, I'd appreciate if you share with me distribution data of these parameters.

Best regards,
Shinichi Yokota