Other Parts Discussed in Thread: INA828
Dear all
we applied to AMC1200, as bleow.
** Question
1. Input Condition : INPUT voltage is DC +50V in U3 and INPUT voltage is DC -50V in U7.
1) First, we have tested U3 in each, It is OK( DC +50V )
Second, we have tested U7 in each, It is OK(DC -50V)
2) But we have tested U3 and U7 when applying DC 50V power at the same time, U3 or U7 is dead(wrong operation)
it is wrong symptoms of U3 and U7 that even if the input is 0v, the amc1200 output is Max.
Please check the circuit and advise to me.
Thanks and BR
PJ