I have a customer using the TLV9064 device.
They have an input voltage of 11.6V max, and this passes through at 43kΩ resistor to the device input.
The voltage at the input is 5.9V, which is beyond the V+ + 0.5 specification in the the "Absolute Maximum Ratings"
However, there is a note (2) which states the voltage at V+ can be higher than this V+ + 0.5V limit, if the current is kept below 10mA.
In their setup, the current would be (11.6 - 5.9) / 43000 = 132uA
(V+ is 5V)
Is this 5.9V allowable, given their current limiting?
Would you have a comment on the high input resistance? (Section 11.1 in the DS mentions: The added resistor contributes thermal noise at the amplifier input and the value must be kept to a minimum in noise-sensitive applications.)
Thanks,
Darren