This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA282: INA 282 for AC current measurement 220VAC low side

Part Number: INA282

Hi! I want to measure alternating currents from 5mA  to 1A from 220VAC and thought of INA282. I want to use it on low side as in the schematic below, is it possible?

The circuit will be "open" until the triac receives signal, then it "closes" for a 300ms time, then "opens" again. It is a circuit to test a differential circuit breaker.

I will use a microcontroller powered by trasnformer and 5V regulator.

Regards,

Martin