Other Parts Discussed in Thread: AFE032
"I need a device for Powerline Communication. I have shortlisted AFE031. This is for airfield lighting system, to communicate with individual lights over power line. The power line is constant current power supply based.
Also let me know if AFE031 can support OFDM? do we need to create a code for that? Or is it inbuilt? Or do we need OFDM at all? MAX2990 is offering OFDM based PLC built-in with no need to code that. There will be hundreds of lights in airfield that's why i was thinking about OFDM. i dont know if we need that or not.
The PLC will primarily to detect the fault in individual lights to the control room, and some important data in CENELAC band using G3/PRIME. Needed solutions are along with the controllers required. either MSP or C2000"
Regards,
Akshat