Other Parts Discussed in Thread: LMG5200
Hello,
- A GaN power switch can operate in the 1st quadrant or the 3rd quadrant if a control signal is given to that switch. That GaN switch can also operate in the 3rd quadrant without 0 control signal to the GaN if the reverse voltage is over 5-7 Volts. Correct?
- Based on that GaN performance BoostXL-3phGaNInv can work as a diode rectifier. Correct?
- If the above is correct does TI have data on how much ripple will be produced at the DC side if BoostXL-3phGaNInv works as a rectifier?
- More specifically, If we use a generator to create a ~40VAC three phase. Can we use BoostXL-3phGaNInv to rectify this to ~40VDC? If so what is the output DC voltage ripple.
Regards
Sam