I have a question related to the input impedance in the following E2E post.
https://e2e.ti.com/support/amplifiers/f/14/p/917744/3391574#3391574
In electrical characteristic table on INA381-Q1 datasheet, there is the specifications of following parameter.
This parameter seems to be explaining the input current flowing into RESET pin.
If so, input impedance range of REST pin is several Mohms range, not 100Mohms range.
How do you think about it?
Regards,
H.Someno
is this parameter