This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

THS7360: 1 to 2 VGA output

Intellectual 1655 points

Replies: 2

Views: 82

Part Number: THS7360

Dir Sir,

    Could we use THS7360 to do dual VGA output with one set of input signals?

    The block diagram is some like below.

     If the answer is yes, do we have any reference circuit for the customer's reference?

     

    

Thanks

Sincerely,

Edward

  • Hello Edward,

    There shouldn't be an issue of using the device in this way, however I don't believe we have any reference circuits in regards to this. Main thing to note here is the different filter properties of the two types of channels and the reduction of the overall input impedance of the device.

    Best,

    Hasan Babiker

  • In reply to Hasan Babiker31:

    Hi Babiker,

        Thanks for your feedback.

        We will try to evaluate the two points you mentioned.

    Thanks

    Sincerely,

    Edward

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.