Hi,
If a 1 MΩ resistor is installed at the input(IN-) of LM2901,
Is there a problem with LM2901 operation?
Customers cannot predict what value the input bias current will be if 1 MΩ is installed.
We expect that the problem with installing a large resistor is that the input offset voltage becomes large.
Please advise on the possible concerns when installing 1 MΩ.
Best regards
Yusuke