This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

OPA350: warm up time required?

Expert 7335 points

Replies: 5

Views: 60

Part Number: OPA350

Hi Team,

Customer is asking if this device has any warm up time requirement so can meet our accuracy/drift spec? Thanks!

Andrew

  • Hi Andrew,

    when looking into the datasheets of OP27, OPA627 and OPA827 I would wait 3...4 minutes after power-on to get full precision of chip. It depends a bit on supply current, supply voltage and load current, or by other words, it depends on the total heat dissipation of chip: The lower the heat dissipation the faster the chip achieves the point where the offset voltage drift becomes marginal.

    Kai

  • In reply to kai klaas69:

    Hi Kai,

    Thanks for the input.

    Customer wants to know if TI ever tested this spec - warm up time to reach specified spec?

    If no, it's ok.

    Per customer's input, some test instruments manual would put a note saying please wait for 30 mins to warm up before using to avoid accuracy problem. My customer also met this kind of problem - warm up time not enough and fail the test. So wants to check around if any requirement for our ICs. 

    Thanks.

    Andrew

     

  • In reply to [FAE] Andrew Wang:

    Hi Andrew, 

    I am requesting the warm up time from the characterization lab. Since this part is designed 20 years ago, it is possible that we may not have such data. I will post it, if we have it. 

    The IC's warm up time per performance specification has to be determined empirically. It is not surprising that a piece of precision equipment may require 30-60 minutes to reach a thermal equilibrium. In an IC level, 5-10 minutes may be required. But in a system level, the warm-up may take a lot longer, as you stated above. So you may ask a customer to determine the pass or fail warm up period empirically. Perform a binary search patterns to determine the warm up threshold time. If the tested equipment passes in X mins, you can perform the same test by reducing the warm up time in X/2 mins etc.. Of course, the warm up periods may be affected by variation in building temperature in different seasons, but the warm up time is typically specified in minimum time. 

    Best,

    Raymond

  • In reply to [FAE] Andrew Wang:

    Hi Andrew,

    how long had the customer to wait until the specification was met?

    Maybe there's another cause for the failing? Is the chip seeing mechanical stress during the testing?

    Kai

  • In reply to kai klaas69:

    Hi Raymond,

    Thanks I already discussed with customer with your good idea, customer can accept it. -)

    Hi Kai,

    Customer doesn't have time to find out exact time need for PASS.  No mechanical stress during test. On the entire signal path, there is one AD8221 has this data shown below. It doesn't look like the root cause though. Customer is still searching it. Thanks!

    Andrew

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.