Other Parts Discussed in Thread: LM7705
The OPA320 is specified from 1.8V to 5.5V with a temperature range of -40 to 125.
Is it possible to use a supply voltage down to 1.71V if the temperatur range is set to 0 to 70 ?
Best Regards
Tor Dag
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi tds
For a single rail, it is not recommended to operate OPA320 below 1.8V per the datasheet recommendation.
However, you may use 1.7V and place a negative supply rail of -0.232V from LM7705. The absolute max. supply voltage Vs = (V+) - (V-) < 6V. LM7705 is a switched capacitor voltage inverter --> input 3-5.25V for positive supply rail, it will generate -0.232V at its output
/cfs-file/__key/communityserver-discussions-components-files/14/OPA320-Low--Vcc-08042020.TSC
If you have any questions, please let us know.
Best,
Raymond