Other Parts Discussed in Thread: TLV7031, LM393LV, SN74LVC2G14, SN74LVC1G14
I have been having a many of failures with the TLV3201 (Single SOT-23-5) comparator trying to Drive LED's continuously around 15 to 20mA ( Operating at 5V).
The data sheet reads short circuit current of 100 mA (source / sink), The Max ratings read " Output short-circuit current - 100mA"
Questions are " Am i driving this device too hard and how much output current can i expect for for driving a load continuously and are there differences in the single/dual versions?
Also i am driving IN- directly from an external circuit with 1.9V (max) with no input limiting resistor. There is a 10mA input max rating to the inputs. As i don't really know what the input circuit looks like could i need some sort of limiting resistor so i I don't exceed the 10mA max input current?
(As information i don't have room on the board to accommodate buffering devices so I was hoping to accomplish this using the comparator alone.)