This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 3
Views: 71
Part Number: INA149
Hi Team,
Do you have the min and max values of input differential impedance of INA149? Datasheet only shows 800 kohm, which is the typical value.
I'm asking this because my customer will need to specify input impedance in their datasheet and now they measured something around 755 kohm, and are not sure if that's reasonable or not.
Thanks!
Roy
-Tamara Alani Learn more about IAs here.
In reply to Tamara M Alani:
Hi Tamara,
By "This means that the absolute value of the resistors between lots fabricated at different times may vary up to +/-15%", is it equivalent to saying that the differential impedance can be in the range of 680 khom to 920 kohm?
Thanks.
In reply to Roy Hsu:
That's correct.