Other Parts Discussed in Thread: THS4561
Hi
We are using THS4551 IC, The output is connected to the 5meter of cable . Is it able to drive the signal to 5meter of cable ?
Regards
Bala
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Michael,
Speed is very less as its input is derived from Hall sensor and cut off frequency of filter (-3db = 270KHz)
THS4551 amplifier output signals are transferred through the shielded differential cable of 5 meter length, not the Twinax also note its not a single cable length, one cable has 2 meter and other one has 3 meter)
ADC is the load, but we have a 2nd order Butterworth filter before the ADC.
I'm attaching the image of THS4551(unity gain), As of now we added 0 ohm series resistor, based on cable impedance series resistor values will be finalized, Can you please check and comment any additional components to be added due to long cable path
Regards
Bala
well you can't drive the cable directly as it looks capacitive, would need the ADC input filter ckt, eventually you need some series output R, an estimate of the cable C or it differential characteristic impedance. You can either do doubly terminated and take a 6dB loss, or treat the cable as a C and work that into your response simulation. You can recover the insertion loss with added gain in the FDA - why use such a fast part, it is very good noise for the power, but you might also look at the THS4561.