This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV9302: replacing TL082 issue

Part Number: TLV9302
Other Parts Discussed in Thread: TL082, TLV9102, TLV9352, , TLV9152

Hi,

my customer was using TL082 to sense the output current of an PSFB converter. 

TL082 is used to sense the current with a shunt resistor placing at ground side(R27).

TL082 is powered by ±5V. The switching frequency of the PSFB is around 120k.

A 5mohm resistor is placed between Isamp1- and AGND.

The customer would like to test some OPA with lower drift to replace TL082.

So we recommended TLV9102, TLV9302, TLV9152, TLV9352.

With TL082, with the same current, the output of TL082 is constant with VOUT increasing.

With TLV9102/9302/9152/9352, and we keep the current constant, the output of the amp will increase along with VOUT increasing, which is not acceptable.

We don’t know what parameter difference between TLV series and TL082 could lead to such new problem. 

Since it's placed at low side, so common mode voltage is almost zero and should not be the cause.