This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB2ANY: Can't find header files for .dll and .lib files provided

Part Number: USB2ANY
Other Parts Discussed in Thread: LP5036EVM,

Hello,

I have to write a small console app (C++ on VS19) that controls the LEDs on a LP5036EVM via USB2ANY.

I've got a .lib and .dll to control the USB2ANY, but no .h file which I can use to include the library into my project. Is a header file available anywhere? I can't seem to find it. And if not, is it possible to use the library without the header file?

And if we're already at it, are there any  code examples out there that I could use as a reference?

Thanks in advance,

SPa