This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] Does TI have integrated 4-20mA transmitters for inputs from bridge sensors?

Intellectual 1775 points

Replies: 1

Views: 59

Does TI have integrated 4-20mA transmitters for inputs from bridge sensors?

Best,

Katlynne Jones

Learn more about XTR products here

  • Yes. When using a bridge sensor, take care that your input signal is properly conditioned. See the attached articles to learn how to use an amplifier with optimized positive feedback to correct for nonlinearities in your sensor. TI's XTR106 includes 2.5V and 5V excitation sources, linearization, and amplification for a bridge sensor input.

    Signal Conditioning and Linearization of RTD Sensors

    Analog Linearization of RTDs

    TI devices: XTR106, PGA309 with XTR117

    The following reference design goes through the theory, component selection, simulation, complete PCB schematic & layout, bill of materials, and measured performance results of a 2-wire (loop-powered) 4-20mA sensor transmitter (XTR117), and PGA309 providing linearization and temperature compensation to a differential bridge sensor voltage. Circuit modifications that help to meet alternate design goals are also discussed.

    TIPD126

    Figure 1 in the XTR106 datasheet + the Applications Information section on page 9 is also a good design reference.

    XTR106 Datasheet: Figure1

    Best,

    Katlynne Jones

    Learn more about XTR products here

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.