This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMC6022: Any changes to LMC6022IMX/NOPB, different DC behave differently

Part Number: LMC6022

Dear Sir/Madam,

MPN: LMC6022IMX/NOPB

We found DC(974R and 02XI) which install at location U7 cannot achieve (slightly lower/marginal) Vout as per customer specification(minimum 2.75V)

The old DC(878V & HLAB) will get higher value (above 2.8 V) as shown in green box. So need to know if there is any changes on this MPN LMC6022IMX/NOPB.

Best regards,

kpk

  • Hello KPK,

    Based on a circuit I have seen, the maximum should be about 3.37V 

    To know what is happening, I need to know the voltages at these test nodes; Pin 5, Pin 6, Pin 7, Potentiometer wiper. 

    Please report this with a suspected bad device and a known good device,