This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Original question:
Question on INA219 calibration register and current LSB
Replies: 2
Views: 34
Part Number: INA260
HI team,Good day. Our customer has INA260 breakout board from Adafruit and they measure the current and power consumption of a motor that draws 5A. The current printed on the screen always end with .00, 0.25, 0.50, 0.75mA. What is the LSB current for the current-power sensors INA169, INA219 and INA260? How they can achieve higher resolution for these devices?Regards,Carlo
Moreover, does the INA169 and INA219 accept current between 0 to 5A?
In reply to Carlo Cabaccan:
Carlo,
The INA260 has an integrated shunt and the current resolution is 1.25mA. So the last digits make sense since they will be multiples of the 0.25.
The INA219 LSB size for current will depend o RShunt selected and conversion time selected and PGA selected gain. With max conversion time 10µV is the LSB size of the shunt voltage.
The INA169 is an analog out and does not have a LSB size.
INA169 is unipolar only so it can measure only currents in one direction and INA219 can measure in both directions. You can use both to measure currents between 0 to 5 A but must select the correct Rshunt resistor.
For greater resolution you can try the INA228 and INA229 but they are currently in preview mode and can only be ordered as samples.
Best Regards,
Javier Contreras, TI Sensing Products Applications Support
Getting Started with Current Sensing Video Training Series
All information in this correspondence and in any related correspondence is provided “as is” and “with all faults”, and it is subject to TI’s Important Notice (http://www.ti.com/corp/docs/legal/important-notice.shtml).