This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 314
Part Number: TLV9151
Hello,
I need to identify replacement op amps for the TS921, TLV271, and AD8665 devices. What are the best P2P(Pin to Pin) replacement amplifiers from TI?
Thanks!
Hi Katherine,
You can consider the TLV9151 in this case, which is a 4.5MHz, 16V, single channel, low Vos and low noise amplifier. It’s RRIO and we also have the dual and quad channel available online if needed.
Here is a table showing the performance differences between TS921, TLV271, AD8665, and the recommended device.
Thank you,
Tim Claycomb