This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS3491RGTEVM: 15V square wave from 3V3

Part Number: THS3491RGTEVM
Other Parts Discussed in Thread: THS3491, UCC27517, UCC27537

Hello

In my project, I try to amplify 3V3 square wave signal (T=100ns %50 DutyCycle) from FPGA. My goal is amplify to signal 15V (>15V, <25V will be enough) amplitude level. I want to see 0-15V square wave on opamp output.

I simulate THS3491 with VCC=25V, VEE=-5V, Rg=200ohm, Rf=1kohm and achive it at 20V. I think my output signal is meet headroom input voltage. But I couldnt understand why I cant get similar result on real pcb. am I missing something?

Appreciate for any help.