Our customer is concerned that the pullup resistors on the SDA and SCL lines will affect the slave address configurations when connecting either or both of the two address pins (A0 and A1) to the SDA or SCL line.
If the voltage on each of the SDA and SCL lines pulled high by the pullup resistors when the bus is idle meets the range of High-level input voltage (VIH) to the two address pins (A0 and A1), can the slave address be configured correctly?
Best regards,
Daisuke