Dear,
I want to use OP07 for temperature sensing using thermocouple and RTD. Measurement point temperature will always be higher than reference point. Hence there won't be negative voltage input. I want to use non inverting amplifier mode. In the OP07 datasheet following information is given.
"The OP07 is powered on when the supply is connected. It can be operated as a single supply operational amplifier or dual supply amplifier depending on the application"
In Layout Example in datasheet, it's also mentioned that pin number 4, i.e.Vcc- can be connected to ground.
Can I use single supply (Only positive) for this application?
Please guide me.
Kind regards,
Krunal Shah.