Other Parts Discussed in Thread: DRV8870
I designed a current sensing circuit based on the LMP8602.
The setup is quite simple:
current sensing resistor is connected to inputs (pins 1, 8)
offset pin is connected to supply as I would like bidirectional measurement
preamplifier goes directly to output amplifier (pins 3-4 shorted).
Supply voltage is +5V at pin 6 (and 7 as already mentioned). ground to pin 2.
As soon as power is provided the output goes to 5V (should be 2.5V).
I suspected some stray voltages at the differential input so as a test shorted the input pins together - output still going to 5V.
What am I missing?