This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMC6484: looking for single channel alternative part.

Part Number: LMC6484
Other Parts Discussed in Thread: LM35, ADS1100, LMC6061, OPA317, OPA388, TLV333, OPA376

Hello,

I'm using LMC6484 to convert a LM35 temperature signal (about 0 - 70° C) into a 0-5 V range which is then fed into an ADS1100. 

I chose the LMC6484 as it was used in a similar existing design ;-)  Now I'm looking for a replacement as I'm only using a single op amp of the LMC6484. It is operated as a single-supply (5V) non-inverting operational amplifier. See attached circuit.

What would be a good replacement, e.g. would a LMC6061 or OPA317 work as a "drop in" replacement? In terms of voltage offset and drift they match or surpass the LMC6484 and I think their lower GBW is of no relevance.

Thanks!