This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/XTR108: how to program it

Part Number: XTR108

Tool/software: TI-RTOS

hello good night, I would like you to help me by providing a basis for how to program this xtr108 q I find it very interesting for your communication spi, (like some ADS11118Q1 that I acquired some time ago), I want to use it for an industrial project for my university for a PT100 from 0 to 300 °, please if you could provide me with a reference code I would be very grateful
  • Hi Fernando,

    At present, we don't have any reference code for the XTR108 using TI-RTOS. That said, the XTR108 datasheet has a complete description of the SPI interface for the XTR108 on page 15, and a detailed design procedure to create an RTD sensor beginning on page 19.

    In order to use the XTR108 for a voltage output (to interface with a typical ADC, for example), you will need to provide a negative voltage between -0.2V and -0.025V at the I_in pin of the XTR, as shown in Figure 14 on page 25. 

  • Fernando

    We haven't heard back from you so we assume this answered your questions. If you need more help just post another reply below.

    Thanks
    Dennis