This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2903-Q1: Saturation voltage

Part Number: LM2903-Q1

Hi team,

I would like to know the saturatoin voltage in our usecase.

Condition:

 Vcc is +5V and +12V

 Isink is 8mA

 Tj is full range

Could you provide me with the data in our conditions?

I hope that it is less than 700mV.

Best regards,

Tomoaki Yoshida 

  • Hi Tomoaki,

    section 6.6 of datasheet says, that VOL can be up to 1.5V at 6mA. So, at 8mA VOL can even be higher.

    A lower VOL can only be achieved with an additional external transistor stage.

    Kai

  • Hello Tomoaki-san,

    Please see Figure 3 in the datasheet, "Output Saturation Voltage".

    This graph shows the output low voltage over current over temperature. Supply voltage makes very little difference.

    So from the graph, 8mA is about 250mV at 125C, well under 700mV. I would avoid currents higher than 8mA, as you start to get into the current limiting range and VOL will start to vary widely.