Dear Team,
Do you have any suggestions on the below schematic?
BR
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Kai,
Thanks for remind.
How about V+ pin, is it necessary to use LDO here?
Currently the customer is using buck here.
BR
Kevin
Hi Kevin,
the voltage output Vout swings from GND to V+. So, if you connect Vout to the input of a microcontroller which is supplied by 3.3V, then it makes sense to also supply the INA210 by 3.3V. The 3.3V supply voltage should be clean and free from any switcher ripple.
Kai
Hi Kevin,
Besides what you and Kai already discussed, you might want to see if the swing to ground limit of 50mV satisfies the requirement coming from the smallest current to be measured. In addition “offset X gain” should be added on top of the 50mV.
Regards, Guang
Hi Kevin,
To you question regarding Fc - It depends on the speed requirement of the application. If full bandwidth is not required such as in DC measurements, then Fc can be placed as low as practical, at a few KHz for example. As Kai replied previously, R is required, not optional, with the capacitor shown for stability reasons.
Thank you Kai for your inputs.
Regards, Guang
Hi Kevin,
I assume your question was answered and will close this thread. If you have further questions please post back.
Regards, Guang