Other Parts Discussed in Thread: INA303
Hello,
We are using the INA303 for short-circuit protection+current sense amplifier.
We are observing a strange phenomenon on the Limit 2 pin of the IC.
There are ripples on this particular pin as opposed to any other pin.
You can refer to the attached oscilloscope snippet.
The probing set-up for the above image is as follows:
Yellow: 5V (Pin no: 1)
Blue: Amplifier output (Pin no: 2)
Magenta: Limit 2 pin (Pin no: 9)
Green: Limit 1 pin (Pin no: 3)
The attached schematic snippet highlights the probes attached with colors on the respective pins and component values
The mathematical details are as follows:
Rshunt: 100uΩ
Sensitivity: 5mV/A (A2 device 50V/V gain)
Limit 1: 316A @ 4.08V. Realized by 51kΩ resistor
Limit 2: -340A @ 0.8V. Realized by 10kΩ resistor
Cdelay: 26.9us. Realized by 100pF capacitor
Reference: 2.5V generated by REF3125AQDBZRQ1
Do you guys have any clues around this issue?
Can you point us to a specific direction to look into?
Thanks!