Other Parts Discussed in Thread: TLV1805, TIDA-020023, TPS1H200A-Q1, ISO1212, CSD87502Q2
Hi, I have to drive an electromagnetic break of a brushless dc motor, it has a rated voltage of 24Vdc and a switch to sense if it's manually activated on not (as it has to be active in order to drive the motor).
I was thinking of the break as a solenoid, and I found TIDA-020023 reference design of TLV1805 in order to drive the break and sense the feedback current, this last parameter would help me to sense the manually activation of the break, because if the break is released, no current would be sensed.
My question is, am I right in selecting this design as a start? Also, I don't need the proportional control, but I suppose that would mean only, that I don't have to change the duty cycle based in the feedback information.
I would appreciate any help or suggestions. Thanks!