Hi Sir,
I have a query about INA186.
There is "the maximum differential input signal times the gain plus VREF is less than the positive swing voltage VSP." in the datasheet.
For example, if gain is 50 V / V, and Vsp is 5V,
can the voltage between V+ ~ V- be normally measured to the current of about 0.1V?
is my thought correct?
In addition, as input differential overload in section 7.4.4.
If the voltage between V+ ~ V- exceeds the range that can be measured normally,
after returning to the normal value, it will output the correct value after 80 us.
This does not fail if the voltage of V+/ V- is less than Absolute maximum rated 42V.
Can I get the correct value in the measurement after 80us?
Thanks.
Regards,