Hi Guys,
Greetings! Our customer need your help to check their circuit issue.
The circuit, at "no current thru shunt" gives an output of 141mV. This, if they have done their calculations correctly, they expect to see a 10.72A.
If they add a load so the shunt current is 500mA, the output raises to 148mV. This is what they expect to see for 11.1A shunt current, so there's an offset.
Why is the part outputting an offset of 141mV ? The output is connected to a Micro-Controller ADC input, with a clamp diode to protect against over-voltage on the ADC input.
Attached schematic: it's a 250A current sensor.
Looking forward to your response. Thanks in advance.
Best regards,
Jonathan