Hi
Can I use an OPA342 in a peak detector circuit like this :
http://en.wikipedia.org/wiki/File:PeakDet.svg
Can it handle an input differential voltage of 5V (with +5V single supply) ?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Can I use an OPA342 in a peak detector circuit like this :
http://en.wikipedia.org/wiki/File:PeakDet.svg
Can it handle an input differential voltage of 5V (with +5V single supply) ?
Thank you.
Hi Remi,
Yes, the OPA342 should work in this application.
The input common-mode voltage range will dictate what the usable input voltage range of the amplifier is. For the OPA342, the input common-mode voltage range is listed as (-0.3V to V+ + 0.3V) so it is a true rail-to-rail input amplifier.
Best Regards,
Collin Wells
Precision Linear Applications