Hi, i'm currently working on a personal project where I have to use ultrasonic transmitters and recievers. For the reciever circuitry I choose INA128 as it provides sufficiant gain in a single stage. In the datasheet (page number 14.15) of INA128 it is told to use a resistor as an input bias current return path. There is no information on how to choose the size of the resistors I am currently using 10Mohm because anything less gives a constant 0 output. When I do not use the resistors I get random noise and when i do, The range is then limmited to a few inches. Can someone help me with this. I am using Jameco 40T/R-12 ultrasnoic pair and the INA is operated at 9v