Hi all,
Would you mind if we ask TPS76850-Q1?
Our customer will use TPS76850-Q1 like as following conditions;
-Conditions-
Input: DC6V
Output: DC5V
Iout: Max 650mA
<Q1>
The datasheet P11 shows Figure14 "TPS76833 DROPOUT VOLTAGE vs FREE-AIR TEMPERATURE".
So, do you have "TPS76850 DROPOUT VOLTAGE vs FREE-AIR TEMPERATURE" with Io=650mA?
Or, if you don't have it, should we explain to our customer to use Vdo=380mV for the design?
<Q2>
How much is the recommended value of following capacitances in above conditions?
-Input capacitance Ci
-Output capacitance Co
And then. if you have some recommended Equivalent series resistance(ESR), could you let us know it?
Kind regards,
Hirotaka Matsumoto