Question: Is it possible to run the AFE4400 on a buffered clock input rather than an external XTAL?
Answer: Yes it is possible to connect a buffered clock input on the Xin pin of AFE4400. This requires that XTALDIS (bit 9) CONTROL2 Register (Reg 0x23h) is set to HIGH.
Question: Why is 8 MHz the only supported frequency?
Answer: The AFE4400 has been characterized for 8MHz frequency only. Running at higher clock frequency will likely affect the ADC in the receive signal chain and impact the performance adversely.
Question: Does TI have any recommendation for a small size 8MHz crystal?
Answer: For a small size crystal, our recommendation is the 8MHz Piezo Ceramic resonator crystal (CSTCE8M00G55-R0) which has the following dimensions (1.3 x 3.2 x 0.7mm)
Question: What is the required accuracy of external clock for AFE4490 (frequency tolerance)?
Response: The AFE4490 can be provided with an external clock that operates at an accuracy of +/-2% around specified value of 8 MHz.