Other Parts Discussed in Thread: DDC232
I am developing a device which will need to measure multiple photodiodes producing current in the 400 fA range, with as much precision as possible. I am investigating the suitability of the DDC232 for this task.
My signals are essentially DC levels, so I can integrate signals for as long as the analog front end IC will allow. The documentation for the DDC232 says that I can integrate for a full second, and that is what I plan to do.
That being said, my device will be battery-powered, and thus it will have very limited power supply choices. If I use a 3.6V lithium battery, I will need to use a PMIC with a boost rail to obtain the 5.0V analog supply for the DDC232, and also to power the 4.096V reference. Is this advisable? The power supply rejection ratio specification for the DDC232 appears to be 100-800 ppm at DC (-40 to -31 dB). Those PSRR numbers don't seem very good to me, but I don't know whether I am interpreting them correctly. If I want to preserve the DDC232's 20 bits (120 dB) of resolution, do I really need to get my power supply noise 80 - 89 dB below my 400 fA signal? That seems impossible to me, even for an LDO. (Of course I will also shield the photodiodes and the DDC232 itself, and pay careful attention to my board layout to minimize noise.)
Thanks for any advice you may have.