Other Parts Discussed in Thread: AFE4400
Hello,
I am designing a wrist HRM based on the AFE4400. Could you recommend me some parts (leds and photodiodes) you have tested and are working fine?
Thanks,
Félix.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: AFE4400
Hello,
I am designing a wrist HRM based on the AFE4400. Could you recommend me some parts (leds and photodiodes) you have tested and are working fine?
Thanks,
Félix.
Hello Felix,
I have attached some of the sensors we have tested below.
| Part number | Mfr. | Type |
| DCM03 | APM Korea | Integrated dual emitter and photodiode |
| APL3015MGC-F01 | Kingbright | Green Led |
| IR17-21C/TR8 | Everlight | IR Led |
| QSB34CGR | Fairchild | Photodiode |
Thanks so much!
I only want to use the HRM capability, not the pulse oximeter. Any recommendation to connect it?
Regards,
Félix.
Hi Praveen,
I have checked the application note which is on the website and I have two hesitates:
- what is the purpose of using the BAV99 and the DLW31? Are they mandatory for HRM applications?
- is it posible to use only one led or it is compulsory to use two LEDs in different bands?
Thanks,
Félix.
Hello Felix,
BAV99W switching diodes are primarily used as diode clamps. If you expect to see accidental higher voltages at the INN, INP, DETP and DETM lines, it is recommended to use clamp diodes to supply and ground to protect the AFE4490 / AFE4400. For battery operated systems this might not be necessary.
DLW31 are EMI suppression filters. In wearable systems with wireless capability, RF energy can attenuate the signals on the INN and INP channels. It is recommended to use the common mode choke coils to suppress common mode noise.
The AFE44xx family of devices supports two LEDs for Pulse Oximetry application. For HRM application, you can use only 1 LED with AFE44xx.
Regards
Praveen.