Other Parts Discussed in Thread: DDC264EVM, DDC264, DDC232
I've just received my DDC264EVM. I am trying to connect it to a 64-bit Windows 7 computer. I believe that I have succeeded in following the directions found at https://e2e.ti.com/support/applications/high_reliability/f/30/t/285994
I want to power the board entirely from USB. When I first plugged the board into the USB port, only LED D1 turned on.
I checked the manual, and saw that I might need to reconfigure some jumpers. I unplugged the board. As recommended in Section 3.1, I opened J19, and shorted J12.
When I turned on the board again, D2, D4, D5, D7, D8 and D14 also lit up. That looks promising.
I followed the driver installation directions in the link mentioned above. Upon completion, my Control Panel > Hardware and Sound > Devices and Printers page shows an EZ-USB device.
I installed the DDC264 Evaluation software. The initial window looks like Figure 13 in the manual, but with "Fast Data" grayed out. When I click the "Refresh All" button, I get the following sequence of messages on the status line: "Hard reset of DDC done", "Wrote FPGA registers (C)", "USB read bus empty", "Reading back CFG register", "Error writing/reading config register". "Fast Data" remains grayed out.
Clicking the "Hard Reset DDC" or "Write CFG / Verify CFG buttons" appear to just perform half of the above tasks each.
Pressing the RESET_USB switch on the board changes the behavior, but not for the better. After I press it, an attempt to "Refresh All" from the software immediately returns the message "Error writing FPGA registers (C)".