Other Parts Discussed in Thread: ADS5263
Hello,
I am trying to determine the full scale input for the 16-bit front end of the ADS5263. The part is advertised as having a 4vpp full scale input while utilizing the 16 bit front end. However the data sheet doesnt really make sense to me. It indicates that the device has a 2vpp full scale in both modes (this is my interpretation)
In the absoule max ratings (section 7.1 of the Rev. D datasheet) The "Voltage applied to analog input pins INP_A, INM_A, INP_B, INM_B" min= 0.3v and max=3.6v or AVDD + 0.3v. Now using these numbers you only have a 3.9vpp swing. I suppose you could look at the max AVDD voltage which = 3.9v and now you could potentially reach a 4.2vpp swing but these are absolute maximum ratings. Furthermore in section 7.3 recomended operatiing conditions the maximum analog supply voltage AVDD = 3.6v with the nominal being 3.3v.
Another confusing section is the analog input section 9.1.1 (rev. D). Taken from the data sheet "The INxP and INxM pins must be externally biased around a common-mode voltage of 1.5 V, available on the VCM pin. For a full-scale differential input, each input pin INP, INM must swing symmetrically between VCM + 1 V and VCM – 1 V, resulting in a 4-Vpp differential input swing." The way I read this is that there is a +-1v swing resulting in a 2vpp swing. Am I missing something?
I called the technical support number and was told that the spec of 4vpp is correct but they couldnt tell me why and refered me to post on this forum to get an answer.
I've read through this data sheet quite a few times and I can't figure this out. Its possible that I'm missing something obious but thats why I'm here.
Thank you for your assistance on this matter!
Ethan